I am using Logic PD AM3517 Experimenter board.
Successfully created and booted MMC/SD card for PSP 04.01.00.00 which uses Kernel 2.6.32 with additions.
I need to get to Kernel 2.6.33.7. When booting from SD card, it successfully uncompresses kernel, loads modules but then hangs with
Waiting for root device /dev/mmcblk0p2...
I see a similar bug report on Kernel 2.6.37 at
http://e2e.ti.com:80/support/dsp/omap_applications_processors/f/447/p/109030/385380.aspx#385380
and a comment by Vaibhav that a PSP 04.02.00.07 release which uses Kernel 2.6.37 fixes this problem.
How can I fix this problem with Kernel 2.6.33.7 and PSP 04.01.00.00?
Thanks