I have a 6467 EVM and it works
ok. Now I have a production board that has 2 6467's in a Jtag Chain and I
cannot get either of them to work with CCS. They seem to check out with
SDconfig though.
SDconfig reports
** Checking for a valid emulator/eZdsp
$$ You are connected to:
$$ EmuProductName=XDS510USB
$$ EmuPortAddr=0x510
$$ EmuPortMode=USB
$$ ProductId=510
$$ ProductVersion=84
** Checking emulator/eZdsp scan connection
** Emulator Test **
$$ EmuProductName=XDS510USB
$$ EmuPortAddr=0x510
$$ EmuPortMode=USB
$$ ProductId=510
$$ ProductVersion=84
** Emulator Scan Test
-- Found JTAG IR length of 12
-- Found 2 JTAG device(s) in the scan chain
And the diagnostics pass with 0 errors.
In code composer Setup I have tried using the 6467 EVM setup and adding another
6467.
I have also tried using the 6467EVm and adding a 6bit bypass.(by pass before
and after the EVM)
I have also tried not using the EVM setup and creating a new board from scratch
and adding 1 6467 and a bypass and tried using 2 6467's.
I set the Arm Gel file to "davincihd_arm.gel" downloaded from
Spectrum Digital.
I have the boot mode set to emulation on both chips.
No matter what I do when I try to connect to the arm I get lots of these
errors.
Trouble Halting Target CPU: Error 0x00000020/-2011 Error during:
Execution, An internal error occurred in which an illegal action
(0x00000000) was requested while disconnected.
Any ideas what the issue could be? I'm assuming that if SDconfig passes then the hardware is connected properly, is this a valid assumption? If so then what could be wrong in the setup?
Thanks
Ringo