This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM365_IPNC SETUP ISSUES

Hi,everyone~~

I'm working on the DM365_IPNC . Yesterday,the IPNC suddenly didn't work,but before yesterday ,it wokred fine.

From the serial :

# ./av_server.out D1 AEWB H264 3000000 CVBR &
#
 AVSERVER UI: Initializing.

DRV_SyncRst: module = 47, domain = 0, state = 0

DRV_SyncRst: module = 47, domain = 0, state = 3
 
 CLK Hz,
 ARM   Hz =  297000000
 DDR   Hz =  243000000
 VPSS  Hz =  243000000
 IMCOP Hz =  243000000
 
 DRV LDC: GetConfig 0004 0x0
 AVSERVER UI: Starting in mode 0
DavinciDisplay DavinciDisplay.1: Before finishing with S_FMT:
layer.pix_fmt.bytesperline = 736,
 layer.pix_fmt.width = 720,
 layer.pix_fmt.height = 480,
 layer.pix_fmt.sizeimage =529920
Rate Control TypDavinciDisplay DavinciDisplay.1: pixfmt->width = 720,
 layer->layer_info.config.line_length= 736
e: IVIDEO_STORAGE ALG: VidEnc: DynamicParams: bitrate = 3000000 bps, Key-frame-interval = 30
 ALG: VidEnc: mbMvOutEnable =1
 ALG: VidEnc: encStatus.bufInfo.minNumOutBufs is 2
 ALG: VidEnc: encStatus.bufInfo.minOutBufSize[0] is 529920
 ALG: VidEnc: encStatus.bufInfo.minOutBufSize[1] is 11040
 ALG: VidEnc: XDM_GETBUFINFO: min in bufs:2 buf(0):353280 buf(1):176640
 ALG: VidEnc: pObj->MV algName =h264enc
 ALG: VidEnc: pObj->MV_Size =11040
 ALG: VidEnc: Default is Disable MV data output
 STREAM: Ext 0: 0x0
 STREAM: Ext 1: 0x0
Creat queue id:98305
queue id:98305
IPNC_1.0 (root@localhost.localdomain) (gcc ç‰æ 4.2.0 (MontaV
IPNC AUTO_IRIS = 1 #####################

 

We can see that it always stops at the red prompt.What's the problem? I rebuild the kernel and the program,the result is the same.

Can anyone help me?

Thanks ~~

Xiang

  • HI,

     

    Firstly, you are using a very old version of software which is close to two years old, please use the latest version 2.6 for IPNC.

     

    On the log, it tough to know the crash details from it, can you give more details about the crash, boot params, boot log etc.

    ALso, is there any changes you did with the lens or whats kind of lens you are using?

     

    Regards,

     

    Raghu

     

  • Thanks for your reply.

    Firstly .I'm using the IPNC v1.0,because I only have the source for this version.How can I get the latest version for IPNC?

    My lens is MT9P031,and I didn't do anything to the lens.

    My bootargs is

    MEM=60M console=ttys1 root=/dev/ram0 rootfstype=cramfs ip=192.168.245.104:255.255.255.0:192.168.245.254 init=0x82000000,12M

    I didn't know the how the crash happen.I execute the program as previos.And it got the problem.

    Why it always stops at the red prompt?Is it anything wrong with the AUTO_IRIS?But for my board ,I didn't connect the DC_IRIS to the dm365.

    Hope for your reply~~

    Thanks~

    Xiang

  • YOu need to connect DC IRIS else you will see the dark video output, please refer to schematic that the feedback is sent via the TVOUT signal.

     

    If you have ordered from Appro directly, you should get the release update notification from them.

    Else please check with source from where you got the IPNC RDK, please ask for the release update from them.

     

    Let me know if you face any issues on it.

     

    Regards,

     

    Raghu