This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi ciyoha,
ciyoha said:Hi all, I have a small but annoying problem. When I open the DSP_BIOS.tcf file in CCStudio v3.3, it was called as a text file. But I want to make it open with the help of Configuration Tool. What are the setting for this should be in CCStudio v3.3?
ciyoha said:When I right click on the TCF file within CCS I do not see DSP/BIOS Config or Graphical Edit. Maybe we have different versions CCS. I use CCS 3,3.
FYI, we've intentionally decoupled the IDE from the other components such as the code generation tools and DSP/BIOS to enable you to upgrade the IDE without affecting the actual code. You should be able to update to the latest version of CCS and install the exact same code generation tools, DSP/BIOS version, etc. to still get the exact same .out file.