This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: 4K H264 encoding support?

Dear Experts,

 Looking at the datasheet of DA4VM, it says :

Video acceleration:
Ultra-HD video, one (3840 × 2160p, 60 fps), or two
(3840 × 2160p, 30 fps) H.264/H.265 decode

Full-HD video, four (1920 × 1080p, 60 fps), or eight
(1920 × 1080p, 30 fps) H.264/H.265 decode

Full-HD video, one (1920 × 1080p, 60 fps), or up to
three (1920 × 1080p, 30 fps) H.264 encode

So could you confirm that it does NOT support H264 encoding for 4K video streaming even for single camera ?

Best Regards,
Khang