Part Number: AM3357
Hello,
I have to use a slave SPI communication on the am3357 chip.
The master signal I receive is uneven. It is generated by software from the client side, and suffers from interrupt, see enclosed document.
The master SPI generates a clock around 700kHz. After 2 bits, the master stops for about 20µs, then resume the last 6 bits.
Because of this delay, I loose completely the transmission. The client cannot change anything on his code (of course).
1) Is there a way to make this kind of transmission work?
2) Is there a register to read if this error occurs, so I can clear the interrupt to start clean all over again?
I thank you in advance,
I wish you an excellent day,
Best regards,
Vincent SERTORIO