Hi all ,
i want to cross compile the Linux kernel without installing the SDK on my system .
i can see that in the latest SDK [ti-processor-sdk-linux-am64xx-evm-08.04.01.04-Linux-x86-Install.bin] 5.10.140 kernel is used. But commit ID of linux kernel that is given in SDK does not match with commit ID given on this direct link https://git.ti.com/cgit/ti-linux-kernel/ti-linux-kernel/tag/?h=v5.10.140 .
I have taken the diff of both version and i have found that there is a significant difference between both the versions of linux kernel although they both claim to be version 5.10.140 .
So my question is which version is more stable ?
How to download the stable 5.10.140 directly git repository without installing the SDK .
I also want to know direct link to download toolchains for kernel and uboot compilation .
Thanks