Part Number: SK-AM62
Hello,
I am using the AM62 SK eva kit with PROCESSOR-SDK-LINUX-AM62 08.04.01.03.
Is it possible to live stream via an Ethernet web camera?
If so, how do I set it up?
Best regards
Magnus
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SK-AM62
Hello,
I am using the AM62 SK eva kit with PROCESSOR-SDK-LINUX-AM62 08.04.01.03.
Is it possible to live stream via an Ethernet web camera?
If so, how do I set it up?
Best regards
Magnus
Hi Magnus,
Could you please help us with your use-case using ethernet webcam? Appreciate if you can share how the camera is being interfaced on AM62x with pics.
This would help me assign this to the rightful owner, for faster response.
With that being said, yes we should be able to live-stream using gstreamer's rtspsrc element provided the camera is functional with all the ethernet interfaces are configured correctly.
Regards,
Suren
Sorry for late answer.
Thanks for guiding me in the right direction.
/Magnus