Part Number: TMDSIDK572
Other Parts Discussed in Thread: AM5729, AM5728, DRA752
1 0
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
** Unable to read file boot.scr **
1490 bytes read in 2 ms (727.5 KiB/s)
Loaded env from uEnv.txt
Importing environment from mmc0 ...
Running uenvcmd ...
1 bytes read in 3 ms (0 Bytes/s)
Already setup.
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
4375040 bytes read in 194 ms (21.5 MiB/s)
90792 bytes read in 6 ms (14.4 MiB/s)
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 8ffe6000, end 8ffff2a7 ... OK
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 4.19.94-rt39-ga242ccf3f1 (oe-user@oe-host) (gcc version 8.3.0 (GNU Toolchain for the A-profile Architecture 8.3-2019.03 (arm-rel-8.36))) #1 SMP PREEMPT RT Sun Apr 19 02:32:36 UTC 2020
[ 0.000000] CPU: ARMv7 Processor [412fc0f2] revision 2 (ARMv7), cr=30c5387d
[ 0.000000] CPU: div instructions available: patching division code
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache
[ 0.000000] OF: fdt: Machine model: TI AM5728 BeagleBoard-X15
[ 0.000000] Memory policy: Data cache writealloc
[ 0.000000] efi: Getting EFI parameters from FDT:
[ 0.000000] efi: UEFI not found.
[ 0.000000] Reserved memory: created CMA memory pool at 0x0000000095800000, size 56 MiB
[ 0.000000] OF: reserved mem: initialized node ipu2-memory@95800000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created CMA memory pool at 0x0000000099000000, size 64 MiB
[ 0.000000] OF: reserved mem: initialized node dsp1-memory@99000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x000000009d000000, size 32 MiB
[ 0.000000] OF: reserved mem: initialized node ipu1-memory@9d000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created CMA memory pool at 0x000000009f000000, size 8 MiB
[ 0.000000] OF: reserved mem: initialized node dsp2-memory@9f000000, compatible id shared-dma-pool
[ 0.000000] cma: Reserved 24 MiB at 0x00000000fe400000
[ 0.000000] OMAP4: Map 0x00000000ffd00000 to (ptrval) for dram barrier
[ 0.000000] Hit pending asynchronous external abort (FSR=0x00001211) during first unmask, this is most likely caused by a firmware/bootloader bug.
[ 0.000000] DRA752 ES2.0
[ 0.000000] random: get_random_bytes called from start_kernel+0xb0/0x488 with crng_init=0
[ 0.000000] percpu: Embedded 15 pages/cpu s32224 r8192 d21024 u61440
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 464192
[ 0.000000] Kernel command line: console=ttyS2,115200n8 root=PARTUUID=062139a4-02 rw rootfstype=ext4 rootwait
[ 0.000000] Dentry cache hash table entries: 131072 (order: 8, 1048576 bytes)
[ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Memory: 1672532K/1863680K available (10240K kernel code, 343K rwdata, 2752K rodata, 2048K init, 276K bss, 35500K reserved, 155648K cma-reserved, 1283072K highmem)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
[ 0.000000] vmalloc : 0xf0800000 - 0xff800000 ( 240 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xf0000000 ( 768 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0x(ptrval) - 0x(ptrval) (12256 kB)
[ 0.000000] .init : 0x(ptrval) - 0x(ptrval) (2048 kB)
[ 0.000000] .data : 0x(ptrval) - 0x(ptrval) ( 344 kB)
[ 0.000000] .bss : 0x(ptrval) - 0x(ptrval) ( 277 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU priority boosting: priority 1 delay 500 ms.
[ 0.000000] No expedited grace period (rcu_normal_after_boot).
[ 0.000000] Tasks RCU enabled.
[ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
[ 0.000000] GIC: Using split EOI/Deactivate mode
[ 0.000000] OMAP clockevent source: timer1 at 32786 Hz
[ 0.000000] arch_timer: cp15 timer(s) running at 6.14MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x16af5adb9, max_idle_ns: 440795202250 ns
[ 0.000005] sched_clock: 56 bits at 6MHz, resolution 162ns, wraps every 4398046511023ns
[ 0.000012] Switching to timer-based delay loop, resolution 162ns
[ 0.000284] clocksource: 32k_counter: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 58327039986419 ns
[ 0.000288] OMAP clocksource: 32k_counter at 32768 Hz
[ 0.000727] Console: colour dummy device 80x30
[ 0.000865] Calibrating delay loop (skipped), value calculated using timer frequency.. 12.29 BogoMIPS (lpj=61475)
[ 0.000873] pid_max: default: 32768 minimum: 301
[ 0.001018] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.001028] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.001733] CPU: Testing write buffer coherency: ok
[ 0.001767] CPU0: Spectre v2: using ICIALLU workaround
[ 0.002006] /cpus/cpu@0 missing clock-frequency property
[ 0.002041] /cpus/cpu@1 missing clock-frequency property
[ 0.002054] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[ 0.059949] Setting up static identity map for 0x80200000 - 0x80200060
[ 0.099980] rcu: Hierarchical SRCU implementation.
[ 0.160238] EFI services will not be available.
[ 0.180118] smp: Bringing up secondary CPUs ...
[ 0.320562] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
[ 0.320567] CPU1: Spectre v2: using ICIALLU workaround
[ 0.320693] smp: Brought up 1 node, 2 CPUs
[ 0.320710] SMP: Total of 2 processors activated (24.59 BogoMIPS).
[ 0.320719] CPU: All CPU(s) started in HYP mode.
[ 0.320726] CPU: Virtualization extensions available.
[ 0.321352] devtmpfs: initialized
[ 0.350520] VFP support v0.3: implementor 41 architecture 4 part 30 variant f rev 0
[ 0.350811] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.350831] futex hash table entries: 512 (order: 3, 32768 bytes)
[ 0.353422] pinctrl core: initialized pinctrl subsystem
[ 0.353993] DMI not present or invalid.
[ 0.354341] NET: Registered protocol family 16
[ 0.355677] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.356585] omap_hwmod: l3_main_2 using broken dt data from ocp
[ 0.558922] OMAP GPIO hardware version 0.1
[ 0.585766] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
[ 0.585779] hw-breakpoint: maximum watchpoint size is 8 bytes.
[ 0.586884] OMAP DMA hardware revision 0.0
[ 0.613138] edma 43300000.edma: memcpy is disabled
[ 0.617306] edma 43300000.edma: TI EDMA DMA engine driver
[ 0.626124] omap-dma-engine 4a056000.dma-controller: OMAP DMA engine driver (LinkedList1/2/3 supported)
[ 0.626940] evm_5v0: supplied by main_12v0
[ 0.630545] omap-iommu 40d01000.mmu: 40d01000.mmu registered
[ 0.630925] omap-iommu 40d02000.mmu: 40d02000.mmu registered
[ 0.631324] omap-iommu 58882000.mmu: 58882000.mmu registered
[ 0.631722] omap-iommu 55082000.mmu: 55082000.mmu registered
[ 0.632255] omap-iommu 41501000.mmu: 41501000.mmu registered
[ 0.632568] omap-iommu 41502000.mmu: 41502000.mmu registered
[ 0.632841] iommu: Adding device 58820000.ipu to group 1
[ 0.632918] iommu: Adding device 55020000.ipu to group 2
[ 0.633033] iommu: Adding device 40800000.dsp to group 0
[ 0.633235] iommu: Adding device 41000000.dsp to group 3
[ 0.634515] SCSI subsystem initialized
[ 0.635623] palmas 0-0058: Irq flag is 0x00000008
[ 0.673335] random: fast init done
[ 0.891646] palmas 0-0058: Muxing GPIO 2b, PWM 0, LED 0
[ 0.897734] SMPS12: supplied by regulator-dummy
[ 0.905529] SMPS3: supplied by regulator-dummy
[ 0.912601] SMPS45: supplied by regulator-dummy
[ 0.921814] SMPS6: supplied by regulator-dummy
[ 0.928025] SMPS7: supplied by regulator-dummy
[ 0.934277] SMPS8: supplied by regulator-dummy
[ 0.935843] smps8: Bringing 1060000uV into 1800000-1800000uV
[ 0.937400] smps8: failed to apply 1800000-1800000uV constraint(-22)
[ 0.937415] palmas-pmic 48070000.i2c:tps659038@58:tps659038_pmic: failed to register 48070000.i2c:tps659038@58:tps659038_pmic regulator
[ 0.938912] palmas-pmic: probe of 48070000.i2c:tps659038@58:tps659038_pmic failed with error -22
[ 0.941082] omap_i2c 48070000.i2c: bus 0 rev0.12 at 400 kHz
[ 0.941941] omap_i2c 48060000.i2c: bus 2 rev0.12 at 400 kHz
[ 0.942282] media: Linux media interface: v0.10
[ 0.942347] videodev: Linux video capture interface: v2.00
[ 0.942479] pps_core: LinuxPPS API ver. 1 registered
[ 0.942489] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.942516] PTP clock support registered
[ 0.942566] EDAC MC: Ver: 3.0.0
[ 0.962137] omap-mailbox 48840000.mailbox: omap mailbox rev 0x400
[ 0.962491] omap-mailbox 48842000.mailbox: omap mailbox rev 0x400
[ 0.963303] Advanced Linux Sound Architecture Driver Initialized.
[ 0.964543] clocksource: Switched to clocksource arch_sys_counter
[ 0.980549] NET: Registered protocol family 2
[ 0.981497] tcp_listen_portaddr_hash hash table entries: 512 (order: 2, 16384 bytes)
[ 0.981562] TCP established hash table entries: 8192 (order: 3, 32768 bytes)
[ 0.981650] TCP bind hash table entries: 8192 (order: 5, 229376 bytes)
[ 0.981969] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.982089] UDP hash table entries: 512 (order: 3, 32768 bytes)
[ 0.982170] UDP-Lite hash table entries: 512 (order: 3, 32768 bytes)
[ 0.982459] NET: Registered protocol family 1
[ 0.993211] RPC: Registered named UNIX socket transport module.
[ 0.993222] RPC: Registered udp transport module.
[ 0.993230] RPC: Registered tcp transport module.
[ 0.993238] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.994693] hw perfevents: no interrupt-affinity property for /pmu, guessing.
[ 0.994954] hw perfevents: enabled with armv7_cortex_a15 PMU driver, 7 counters available
[ 0.996599] Initialise system trusted keyrings
[ 0.996785] workingset: timestamp_bits=14 max_order=19 bucket_order=5
[ 1.006128] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 1.006957] NFS: Registering the id_resolver key type
[ 1.006984] Key type id_resolver registered
[ 1.006995] Key type id_legacy registered
[ 1.007065] ntfs: driver 2.1.32 [Flags: R/O].
[ 1.009687] Key type asymmetric registered
[ 1.009700] Asymmetric key parser 'x509' registered
[ 1.009795] bounce: pool size: 64 pages
[ 1.009847] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245)
[ 1.009858] io scheduler noop registered
[ 1.009867] io scheduler deadline registered
[ 1.010177] io scheduler cfq registered (default)
[ 1.010188] io scheduler mq-deadline registered
[ 1.010197] io scheduler kyber registered
[ 1.018187] pinctrl-single 4a003400.pinmux: 282 pins, size 1128
[ 1.023519] dra7-pcie 51000000.pcie: Linked as a consumer to phy-4a094000.pciephy.1
[ 1.024166] dra7-pcie 51000000.pcie: host bridge /ocp/axi@0/pcie@51000000 ranges:
[ 1.024230] dra7-pcie 51000000.pcie: IO 0x20003000..0x20012fff -> 0x00000000
[ 1.024259] dra7-pcie 51000000.pcie: MEM 0x20013000..0x2fffffff -> 0x20013000
[ 1.254003] random: crng init done
[ 2.014860] dra7-pcie 51000000.pcie: Phy link never came up
[ 2.015077] dra7-pcie 51000000.pcie: PCI host bridge to bus 0000:00
[ 2.015099] pci_bus 0000:00: root bus resource [bus 00-ff]
[ 2.015134] pci_bus 0000:00: root bus resource [io 0x0000-0xffff]
[ 2.015146] pci_bus 0000:00: root bus resource [mem 0x20013000-0x2fffffff]
[ 2.021539] PCI: bus0: Fast back to back transfers disabled
[ 2.027369] PCI: bus1: Fast back to back transfers enabled
[ 2.027416] pci 0000:00:00.0: BAR 0: assigned [mem 0x20100000-0x201fffff 64bit]
[ 2.027452] pci 0000:00:00.0: PCI bridge to [bus 01-ff]
[ 2.028114] pcieport 0000:00:00.0: Signaling PME with IRQ 170
[ 2.028465] pcieport 0000:00:00.0: AER enabled with IRQ 170
[ 2.125661] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled
[ 2.130743] console [ttyS2] disabled
[ 2.130830] 48020000.serial: ttyS2 at MMIO 0x48020000 (irq = 45, base_baud = 3000000) is a 8250
[ 3.195585] console [ttyS2] enabled
[ 3.202049] omap_rng 48090000.rng: Random Number Generator ver. 20
[ 3.230023] brd: module loaded
[ 3.244128] loop: module loaded
[ 3.252910] libphy: Fixed MDIO Bus: probed
[ 3.314623] davinci_mdio 48485000.mdio: davinci mdio revision 1.6, bus freq 1000000
[ 3.322323] libphy: 48485000.mdio: probed
[ 3.330088] mdio_bus 48485000.mdio: MDIO device at address 2 is missing.
[ 3.336841] davinci_mdio 48485000.mdio: phy[1]: device 48485000.mdio:01, driver Micrel KSZ9031 Gigabit PHY
[ 3.347286] cpsw 48484000.ethernet: Detected MACID = e4:15:f6:0d:fa:d2
[ 3.353970] cpsw 48484000.ethernet: initialized cpsw ale version 1.4
[ 3.360359] cpsw 48484000.ethernet: ALE Table size 1024
[ 3.365674] cpsw 48484000.ethernet: cpts: overflow check period 500 (jiffies)
[ 3.374274] cpsw 48484000.ethernet: cpsw: Detected MACID = e4:15:f6:0d:fa:d3
[ 3.383679] i2c /dev entries driver
[ 3.394766] gpio-fan gpio_fan: GPIO fan initialized
[ 3.400869] tmp102 0-0048: error reading config register
[ 3.406376] tmp102: probe of 0-0048 failed with error -121
[ 3.414982] sdhci: Secure Digital Host Controller Interface driver
[ 3.421199] sdhci: Copyright(c) Pierre Ossman
[ 3.426735] sdhci-pltfm: SDHCI platform and OF driver helper
[ 3.433698] omap_gpio 4805d000.gpio: Could not set line 27 debounce to 200000 microseconds (-22)
[ 3.442538] sdhci-omap 4809c000.mmc: Got CD GPIO
[ 3.447514] sdhci-omap 4809c000.mmc: Linked as a consumer to regulator.12
[ 3.454374] sdhci-omap 4809c000.mmc: 4809c000.mmc supply vqmmc not found, using dummy regulator
[ 3.463231] sdhci-omap 4809c000.mmc: Linked as a consumer to regulator.0
[ 3.470090] sdhci-omap 4809c000.mmc: Dropping the link to regulator.0
[ 3.476756] sdhci-omap 4809c000.mmc: Dropping the link to regulator.12
[ 3.484060] sdhci-omap 480b4000.mmc: failed to set system capabilities
[ 3.501763] l4per_cm:clk:0168:0: failed to enable
[ 3.506518] ------------[ cut here ]------------
[ 3.506532] ------------[ cut here ]------------
[ 3.506547] WARNING: CPU: 1 PID: 59 at drivers/clk/clk.c:828 clk_core_disable+0xa4/0xa8
[ 3.506551] l4per_cm:clk:0168:0 already disabled
[ 3.506554] Modules linked in:
[ 3.506565] CPU: 1 PID: 59 Comm: kworker/1:1 Not tainted 4.19.94-rt39-ga242ccf3f1 #1
[ 3.506567] Hardware name: Generic DRA74X (Flattened Device Tree)
[ 3.506582] Workqueue: pm pm_runtime_work
[ 3.506586] Backtrace:
[ 3.506598] [<c020c6a4>] (dump_backtrace) from [<c020c9dc>] (show_stack+0x18/0x1c)
[ 3.506604] r7:c0e00a50 r6:60000113 r5:00000000 r4:c1253d1c
[ 3.506614] [<c020c9c4>] (show_stack) from [<c09f248c>] (dump_stack+0x9c/0xb0)
[ 3.506626] [<c09f23f0>] (dump_stack) from [<c022d120>] (__warn+0xdc/0xf8)
[ 3.506631] r7:c0e00a50 r6:00000009 r5:00000000 r4:eebfdcfc
[ 3.506641] [<c022d044>] (__warn) from [<c022cd30>] (warn_slowpath_fmt+0x50/0x6c)
[ 3.506647] r9:eebfdd88 r8:00000000 r7:00000020 r6:c1213210 r5:c0e00bec r4:c1207488
[ 3.506656] [<c022cce4>] (warn_slowpath_fmt) from [<c05c103c>] (clk_core_disable+0xa4/0xa8)
[ 3.506659] r3:ee83b780 r2:c0e00bec
[ 3.506663] r5:c12563c8 r4:ee839a80
[ 3.506669] [<c05c0f98>] (clk_core_disable) from [<c05c1834>] (clk_core_disable_lock+0x1c/0x24)
[ 3.506672] r5:c12563c8 r4:ee839a80
[ 3.506680] [<c05c1818>] (clk_core_disable_lock) from [<c05c1860>] (clk_disable+0x24/0x28)
[ 3.506683] r5:c12563c8 r4:c1213210
[ 3.506691] [<c05c183c>] (clk_disable) from [<c021cb80>] (_disable_clocks+0x20/0x98)
[ 3.506698] [<c021cb60>] (_disable_clocks) from [<c021d768>] (_idle+0x188/0x248)
[ 3.506702] r7:00000020 r6:c1207488 r5:c12563c8 r4:c1213210
[ 3.506710] [<c021d5e0>] (_idle) from [<c021f404>] (omap_hwmod_idle+0x28/0x44)
[ 3.506716] r9:c1207488 r8:c021fe98 r7:c1205100 r6:00000001 r5:c121325c r4:c1213210
[ 3.506723] [<c021f3dc>] (omap_hwmod_idle) from [<c021fe44>] (omap_device_idle+0x48/0x9c)
[ 3.506727] r5:eeab8d40 r4:00000000
[ 3.506734] [<c021fdfc>] (omap_device_idle) from [<c021febc>] (_od_runtime_suspend+0x24/0x28)
[ 3.506738] r7:c1205100 r6:eeac5688 r5:00000000 r4:eeac5610
[ 3.506747] [<c021fe98>] (_od_runtime_suspend) from [<c06bf374>] (__rpm_callback+0xe4/0x1c0)
[ 3.506751] r5:00000000 r4:eeac5610
[ 3.506760] [<c06bf290>] (__rpm_callback) from [<c06bf478>] (rpm_callback+0x28/0x88)
[ 3.506766] r10:ffffe000 r9:c1207488 r8:00000008 r7:c1205100 r6:c021fe98 r5:00000000
[ 3.506768] r4:eeac5610
[ 3.506777] [<c06bf450>] (rpm_callback) from [<c06be508>] (rpm_suspend+0x148/0x518)
[ 3.506781] r7:c1205100 r6:c021fe98 r5:00000000 r4:eeac5610
[ 3.506790] [<c06be3c0>] (rpm_suspend) from [<c06bea5c>] (rpm_idle+0xc8/0x148)
[ 3.506796] r10:00000000 r9:eeac56c0 r8:eeac56cc r7:00000000 r6:00000002 r5:00000000
[ 3.506798] r4:eeac5610
[ 3.506807] [<c06be994>] (rpm_idle) from [<c06bfc24>] (pm_runtime_work+0xa4/0xa8)
[ 3.506813] r9:eeac56c0 r8:00000000 r7:eed6d000 r6:eeac5610 r5:eeac5688 r4:eeac56bc
[ 3.506824] [<c06bfb80>] (pm_runtime_work) from [<c02459f0>] (process_one_work+0x1f4/0x404)
[ 3.506829] r7:eed6d000 r6:eed68c80 r5:eea03880 r4:eeac56bc
[ 3.506837] [<c02457fc>] (process_one_work) from [<c0246ff0>] (worker_thread+0x58/0x56c)
[ 3.506842] r10:eea03880 r9:eed68c80 r8:c1205100 r7:eed68c98 r6:00000008 r5:eed68c80
[ 3.506845] r4:eea03894
[ 3.506853] [<c0246f98>] (worker_thread) from [<c024c27c>] (kthread+0x160/0x168)
[ 3.506858] r10:ee8ede74 r9:c0246f98 r8:eea03880 r7:eebfc000 r6:00000000 r5:eea04600
[ 3.506861] r4:eebcd8c0
[ 3.506869] [<c024c11c>] (kthread) from [<c02010e0>] (ret_from_fork+0x14/0x34)
[ 3.506872] Exception stack(0xeebfdfb0 to 0xeebfdff8)
[ 3.506877] dfa0: 00000000 00000000 00000000 00000000
[ 3.506882] dfc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 3.506886] dfe0: 00000000 00000000 00000000 00000000 00000013 00000000
[ 3.506892] r10:00000000 r9:00000000 r8:00000000 r7:00000000 r6:00000000 r5:c024c11c
[ 3.506894] r4:eea04600
[ 3.506897] ---[ end trace 0000000000000001 ]---
[ 3.506921] davinci-mcasp 48468000.mcasp: ERRATA i868 workaround is enabled
[ 3.508938] l4per_cm:clk:0168:0: failed to enable
[ 3.508972] ------------[ cut here ]------------
[ 3.508982] WARNING: CPU: 1 PID: 59 at drivers/clk/clk.c:828 clk_core_disable+0xa4/0xa8
[ 3.508985] l4per_cm:clk:0168:0 already disabled
[ 3.508987] Modules linked in:
[ 3.508996] CPU: 1 PID: 59 Comm: kworker/1:1 Tainted: G W 4.19.94-rt39-ga242ccf3f1 #1
[ 3.508999] Hardware name: Generic DRA74X (Flattened Device Tree)
[ 3.509008] Workqueue: pm pm_runtime_work
[ 3.509012] Backtrace:
[ 3.509021] [<c020c6a4>] (dump_backtrace) from [<c020c9dc>] (show_stack+0x18/0x1c)
[ 3.509026] r7:c0e00a50 r6:60000113 r5:00000000 r4:c1253d1c
[ 3.509034] [<c020c9c4>] (show_stack) from [<c09f248c>] (dump_stack+0x9c/0xb0)
[ 3.509044] [<c09f23f0>] (dump_stack) from [<c022d120>] (__warn+0xdc/0xf8)
[ 3.509048] r7:c0e00a50 r6:00000009 r5:00000000 r4:eebfdcfc
[ 3.509058] [<c022d044>] (__warn) from [<c022cd30>] (warn_slowpath_fmt+0x50/0x6c)
[ 3.509064] r9:eebfdd88 r8:00000000 r7:00000020 r6:c1213210 r5:c0e00bec r4:c1207488
[ 3.509072] [<c022cce4>] (warn_slowpath_fmt) from [<c05c103c>] (clk_core_disable+0xa4/0xa8)
[ 3.509075] r3:ee83b780 r2:c0e00bec
[ 3.509079] r5:c12563c8 r4:ee839a80
[ 3.509085] [<c05c0f98>] (clk_core_disable) from [<c05c1834>] (clk_core_disable_lock+0x1c/0x24)
[ 3.509088] r5:c12563c8 r4:ee839a80
[ 3.509095] [<c05c1818>] (clk_core_disable_lock) from [<c05c1860>] (clk_disable+0x24/0x28)
[ 3.509099] r5:c12563c8 r4:c1213210
[ 3.509105] [<c05c183c>] (clk_disable) from [<c021cb80>] (_disable_clocks+0x20/0x98)
[ 3.509111] [<c021cb60>] (_disable_clocks) from [<c021d768>] (_idle+0x188/0x248)
[ 3.509115] r7:00000020 r6:c1207488 r5:c12563c8 r4:c1213210
[ 3.509122] [<c021d5e0>] (_idle) from [<c021f404>] (omap_hwmod_idle+0x28/0x44)
[ 3.509128] r9:c1207488 r8:c021fe98 r7:c1205100 r6:00000001 r5:c121325c r4:c1213210
[ 3.509135] [<c021f3dc>] (omap_hwmod_idle) from [<c021fe44>] (omap_device_idle+0x48/0x9c)
[ 3.509138] r5:eeab8d40 r4:00000000
[ 3.509145] [<c021fdfc>] (omap_device_idle) from [<c021febc>] (_od_runtime_suspend+0x24/0x28)
[ 3.509150] r7:c1205100 r6:eeac5688 r5:00000000 r4:eeac5610
[ 3.509158] [<c021fe98>] (_od_runtime_suspend) from [<c06bf374>] (__rpm_callback+0xe4/0x1c0)
[ 3.509161] r5:00000000 r4:eeac5610
[ 3.509170] [<c06bf290>] (__rpm_callback) from [<c06bf478>] (rpm_callback+0x28/0x88)
[ 3.509175] r10:ffffe000 r9:c1207488 r8:00000008 r7:c1205100 r6:c021fe98 r5:00000000
[ 3.509178] r4:eeac5610
[ 3.509187] [<c06bf450>] (rpm_callback) from [<c06be508>] (rpm_suspend+0x148/0x518)
[ 3.509191] r7:c1205100 r6:c021fe98 r5:00000000 r4:eeac5610
[ 3.509200] [<c06be3c0>] (rpm_suspend) from [<c06bea5c>] (rpm_idle+0xc8/0x148)
[ 3.509205] r10:00000000 r9:eeac56c0 r8:eeac56cc r7:00000000 r6:00000002 r5:00000000
[ 3.509207] r4:eeac5610
[ 3.509216] [<c06be994>] (rpm_idle) from [<c06bfc24>] (pm_runtime_work+0xa4/0xa8)
[ 3.509222] r9:eeac56c0 r8:00000000 r7:eed6d000 r6:eeac5610 r5:eeac5688 r4:eeac56bc
[ 3.509231] [<c06bfb80>] (pm_runtime_work) from [<c02459f0>] (process_one_work+0x1f4/0x404)
[ 3.509236] r7:eed6d000 r6:eed68c80 r5:eea03880 r4:eeac56bc
[ 3.509244] [<c02457fc>] (process_one_work) from [<c0246ff0>] (worker_thread+0x58/0x56c)
[ 3.509249] r10:eea03880 r9:eed68c80 r8:c1205100 r7:eed68c98 r6:00000008 r5:eed68c80
[ 3.509252] r4:eea03894
[ 3.509259] [<c0246f98>] (worker_thread) from [<c024c27c>] (kthread+0x160/0x168)
[ 3.509264] r10:ee8ede74 r9:c0246f98 r8:eea03880 r7:eebfc000 r6:00000000 r5:eea04600
[ 3.509266] r4:eebcd8c0
[ 3.509273] [<c024c11c>] (kthread) from [<c02010e0>] (ret_from_fork+0x14/0x34)
[ 3.509277] Exception stack(0xeebfdfb0 to 0xeebfdff8)
[ 3.509281] dfa0: 00000000 00000000 00000000 00000000
[ 3.509286] dfc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 3.509290] dfe0: 00000000 00000000 00000000 00000000 00000013 00000000
[ 3.509295] r10:00000000 r9:00000000 r8:00000000 r7:00000000 r6:00000000 r5:c024c11c
[ 3.509297] r4:eea04600
[ 3.509300] ---[ end trace 0000000000000002 ]---
[ 3.510320] NET: Registered protocol family 10
[ 3.535251] Segment Routing with IPv6
[ 3.535328] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[ 3.535931] NET: Registered protocol family 17
[ 3.536171] Key type dns_resolver registered
[ 3.536316] Registering SWP/SWPB emulation handler
[ 3.536322] omap_voltage_late_init: Voltage driver support not added
[ 3.536325] Power Management for TI OMAP4+ devices.
[ 3.537234] Loading compiled-in X.509 certificates
[ 3.579328] dmm 4e000000.dmm: workaround for errata i878 in use
[ 3.684586] dmm 4e000000.dmm: timed out waiting for done
[ 3.684594] dmm 4e000000.dmm: refill failed
[ 3.794599] dmm 4e000000.dmm: timed out waiting for done
[ 3.794606] dmm 4e000000.dmm: refill failed
[ 3.794612] dmm 4e000000.dmm: initialized all PAT entries
[ 3.796762] omap_gpio 4805d000.gpio: Could not set line 27 debounce to 200000 microseconds (-22)
[ 3.796769] sdhci-omap 4809c000.mmc: Got CD GPIO
[ 3.797014] sdhci-omap 4809c000.mmc: Linked as a consumer to regulator.12
[ 3.797071] sdhci-omap 4809c000.mmc: 4809c000.mmc supply vqmmc not found, using dummy regulator
[ 3.797144] sdhci-omap 4809c000.mmc: Linked as a consumer to regulator.0
[ 3.797236] sdhci-omap 4809c000.mmc: Dropping the link to regulator.0
[ 3.797391] sdhci-omap 4809c000.mmc: Dropping the link to regulator.12
[ 3.798206] sdhci-omap 480b4000.mmc: failed to set system capabilities
[ 3.799198] omap_gpio 4805d000.gpio: Could not set line 27 debounce to 200000 microseconds (-22)
[ 3.799203] sdhci-omap 4809c000.mmc: Got CD GPIO
[ 3.799413] sdhci-omap 4809c000.mmc: Linked as a consumer to regulator.12
[ 3.799464] sdhci-omap 4809c000.mmc: 4809c000.mmc supply vqmmc not found, using dummy regulator
[ 3.799536] sdhci-omap 4809c000.mmc: Linked as a consumer to regulator.0
[ 3.799618] sdhci-omap 4809c000.mmc: Dropping the link to regulator.0
[ 3.799759] sdhci-omap 4809c000.mmc: Dropping the link to regulator.12
[ 3.800545] sdhci-omap 480b4000.mmc: failed to set system capabilities
[ 3.801550] hctosys: unable to open rtc device (rtc0)
[ 3.802343] ALSA device list:
[ 3.802346] No soundcards found.
[ 4.456356] WARNING: CPU: 0 PID: 31 at drivers/bus/omap_l3_noc.c:147 l3_interrupt_handler+0x330/0x380
[ 4.456367] 44000000.ocp:L3 Custom Error: MASTER MPU TARGET L4_PER2_P3 (Idle): Data Access in Supervisor mode during Functional access
[ 4.456370] Modules linked in:
[ 4.456381] CPU: 0 PID: 31 Comm: irq/23-l3-app-i Tainted: G W 4.19.94-rt39-ga242ccf3f1 #1
[ 4.456383] Hardware name: Generic DRA74X (Flattened Device Tree)
[ 4.456386] Backtrace:
[ 4.456399] [<c020c6a4>] (dump_backtrace) from [<c020c9dc>] (show_stack+0x18/0x1c)
[ 4.456407] r7:c0df4754 r6:60000113 r5:00000000 r4:c1253d1c
[ 4.456417] [<c020c9c4>] (show_stack) from [<c09f248c>] (dump_stack+0x9c/0xb0)
[ 4.456428] [<c09f23f0>] (dump_stack) from [<c022d120>] (__warn+0xdc/0xf8)
[ 4.456434] r7:c0df4754 r6:00000009 r5:00000000 r4:eea59e24
[ 4.456444] [<c022d044>] (__warn) from [<c022cd30>] (warn_slowpath_fmt+0x50/0x6c)
[ 4.456450] r9:ee9f0c40 r8:f0882564 r7:c0df4680 r6:c0df45c0 r5:c0df4724 r4:c1207488
[ 4.456460] [<c022cce4>] (warn_slowpath_fmt) from [<c0556f24>] (l3_interrupt_handler+0x330/0x380)
[ 4.456464] r3:ee9f3480 r2:c0df4724
[ 4.456468] r5:00000000 r4:80080003
[ 4.456479] [<c0556bf4>] (l3_interrupt_handler) from [<c0289f0c>] (irq_forced_thread_fn+0x28/0xa0)
[ 4.456485] r10:00000001 r9:c0289ee4 r8:00000000 r7:ffffe000 r6:ee9f38a4 r5:ee9f3880
[ 4.456487] r4:ee879800
[ 4.456496] [<c0289ee4>] (irq_forced_thread_fn) from [<c028a2e4>] (irq_thread+0x140/0x22c)
[ 4.456500] r7:ffffe000 r6:ee9f38a4 r5:ee9f3880 r4:ee879800
[ 4.456510] [<c028a1a4>] (irq_thread) from [<c024c27c>] (kthread+0x160/0x168)
[ 4.456515] r10:ee88fa94 r9:c028a1a4 r8:ee9f3880 r7:eea58000 r6:00000000 r5:ee9f38c0
[ 4.456518] r4:ee9fa080
[ 4.456526] [<c024c11c>] (kthread) from [<c02010e0>] (ret_from_fork+0x14/0x34)
[ 4.456529] Exception stack(0xeea59fb0 to 0xeea59ff8)
[ 4.456534] 9fa0: 00000000 00000000 00000000 00000000
[ 4.456539] 9fc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 4.456543] 9fe0: 00000000 00000000 00000000 00000000 00000013 00000000
[ 4.456549] r10:00000000 r9:00000000 r8:00000000 r7:00000000 r6:00000000 r5:c024c11c
[ 4.456551] r4:ee9f38c0
[ 4.456555] ---[ end trace 0000000000000004 ]---
[ 4.666102] Waiting for root device PARTUUID=062139a4-02...
[ 34.394668] vdd_3v3: disabling
[ 34.397746] aic_dvdd_fixed: disabling
[ 34.401435] pbias_mmc_omap5: disabling
Hi,
I have installed the RT-Linux Processor SDK in windows and used win32 disk imager to write the image file into the sdcard. After inserting the sdcard into the eval board.
I am checking the serial console and able to get the datas which i will attach as a log. In that it is showing hardware board as DRA instead of AM5729.Please check that. Also I am not able to proceed further in that sdk .Am not getting any response in that console. Please suggest it.The Uart is connected to the Windows host machine.
.Instead of getting Data Output from serial console, What are the steps that has to be done to check the output via HDMI/Monitor. Please suggest the necessary details.
Thanks,
Thilak