This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Upstream patch of USB on DM356



This patch enables USB on DM365 for last Linux kernels from 2.6.33 to current 3.0.0-rc and.

http://www.makelinux.net/kernel/patches/linux-2.6.33-3.0.0-dm365-usb.patch

Actually the patch is upstreaming patches 0417-DaVinci-DM365-Enable-USB-in-DM365-EVM.patch and 0418-USB-DaVinci-Add-DM365-support-to-DaVinci-USB-drive.patch from DaVinci-PSP-SDK 03.21.00.04

The patch tested on kernels from kernel.org and http://gitorious.org/linux-davinci.

The latest kernels have webcam usb gabget implementation. With this patch it allows to stream video from DM365 to PC via USB.

You are welcome to test and validate the patch before submitting to kernel.org