Hello
I
have bought a DM648 and currently working on the project helloworld
placed on the following path
dvsdk_1_10_00_26_DM648\ndk_1_92_00_22_eval.
I have the following topology configured :
computer A -> Ethernet Physical 0 --- Board --- Ethernet Physical 1 -> computer B
The
above project in it true form full duplex communication between the two
ports. I have placed break points in different location of the code but
it never enters or stop at the break point in the function HwpacketNext.
I
changed the mode to Ale bypass mode , only sided communication was
established meaning the packets of Computer A were being received and
passed to computer B . But the packets of computer B were not being
received or send to computer A . Furthermore the packets received from
computer A was forwarded not only to computer B but was also send to
computer A as well.
kindly i need your help , please
comment how can i make both computer communicate in ALE bypass mode. N
how to stop the board from retransmitting the packet back to prot from
which it has received the packet.
Please reply asap , i would be most grateful
Thank you
waiting for a reply
Amna