Other Parts Discussed in Thread: SYSCONFIG
My last question is here:
http://e2e.ti.com/support/dsp/omap_applications_processors/f/447/p/113720/402967.aspx#402967
and my code still doesn't work yet :-(
here is my code:
#define MY_CS 4
#define SLV_NUM 1
static void __iomem *gpmc_base;
static void __iomem *gpmc_cs4_base=0;
unsigned long cs4_mem_base;
static u32 gpmc_read_reg(int idx)
{
return __raw_readl(gpmc_base + idx);
}
static void gpmc_write_reg(int idx, u32 val)
{
__raw_writel(val, gpmc_base + idx);
}
u32 read_from_mcb(int idx)
{
return __raw_readl(gpmc_cs4_base+idx*4);
}
void write_to_mcb(int idx, u32 val)
{
__raw_writel(val, gpmc_cs4_base+ idx*4);
}
int my_gpmc_init()
{
gpmc_write_reg(GPMC_SYSCONFIG, 0x18);
gpmc_write_reg(GPMC_CONFIG, 0x12);
//sychronous,16bit,NOR,no multiplexed,GPMC_CLK==GPMC_FCLK
gpmc_cs_write_reg(MY_CS, GPMC_CS_CONFIG1,0x28001000);
if (gpmc_cs_request(MY_CS, SZ_16M, &cs4_mem_base) < 0)
{
printk("<1>Failed to request GPMC mem for cs4\n");
return -1;
}
printk("<1>cs4_mem_base:%x\n",cs4_mem_base);
gpmc_cs4_base=ioremap(cs4_mem_base,SZ_16M);
return 0;
}
void mcb_init(void)
{
u32 i;
int offset=0;
//off mcb
write_to_mcb(1, 0);
//mcb configure
write_to_mcb(0, 1);//comm.m_s = 1;
write_to_mcb(3, SLV_NUM);//comm.slv_num = 1;
write_to_mcb(4, 5);//comm.t_cyclic = 5; //500us
for(i = 0; i < SLV_NUM; i++)
{
offset = 112 + i*50;
write_to_mcb(offset, (i+3)<<8);//addr.addr_s = (i+3)<<8;
write_to_mcb(offset+1, DA_M1);//addr.addr_m = DA_M1;
}
//on mcb
write_to_mcb(1, 1);
printk("<1>read back checking......\n");
printk("<1>on:%lu(1)\nm_s:%lu(1)\nslv_num:%lu(1)\nt_cyclic:%lu(5)\n",read_from_mcb(1),read_from_mcb(0),read_from_mcb(3),read_from_mcb(4));
}
int init_module(void)
{
int ret;
u32 l;
unsigned long rate;
l = OMAP34XX_GPMC_BASE;
gpmc_base = ioremap(l, SZ_4K);
my_gpmc_init();
if(gpmc_cs4_base!=0)
{
printk("<1>gpmc_cs4_base:%x",gpmc_cs4_base);
mcb_init();
}
return 1;
}
void cleanup_module(void)
{
printk("<1>cleanup module ......\n");
}
As you see,in function mcb_init(void),I write data to the FPGA and read them back for checking.
The expected results should be "1,1,1,5" but they turn out to be all zero!
Have I done anything wrong?
In 《omap35xx-Technical Reference Manual》there is a note:
When the GPMC is configured for synchronous mode, the GPMC_CLK signal (which is an
output) must also be set as an input (CONTROL.CONTROL_PADCONF_GPMC_NCS7[24]
INPUTENABLE1 = 1). GPMC_CLK is looped back through the output and input buffers of
the corresponding GPMC_CLK pad at the OMAP boundary. The looped-back clock is used
to synchronize the sampling of the memory signals.
What does it mean?What shall I do in my code?
thankyou very much.