This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6474 SRIO Boot mode

Hi:

I encounter a problem in the C6474`s SRIO boot mode.After the c6474 is configured with SRIO boot mode, I read the SRIO register,the result is as follows:

(0x1060)BASE_ID=0x00030003,

(0x0080)DEVICE_ID=0x00ffffff(I do not known why it is not equal to the BASE_ID )

(0x0280)Doorbell0_ICRR=0x0000(I do not known why it is not ox44444444 as the bootloader `PDF).

Because  the DEVICE_ID is not equal to the BASE_ID, I want to write a maintenance packet to the DEVICEID_REG1,what is the destination address I should write?0x80?or else?

when reading the BASE_ID,the result is 0x00 rather than 0x00030003? I do not known why?

I am eager for your reply,thanks for your attention!

xiaoyan