Part Number: AMIC110
Hi Sir/Madam,
I am developing a project with UART module of AMIC110.
Now URAT0, UART1, and UART3 are already configured and work well.
The issue I have is UART2.
The console always shows CortxA8: Unhandled ADP_Stopped exception 0x801F9970, when the program executes the line of uart_handler = UART_open(2, ¶ms);
UART_open() is in the line 16 of the attached code blow.
Because the configuration I did for UART2 is the same as for UART0/1/3, I am confused why UART2 cannot open, even it makes the system crash during opening.
After opening UART2, I need UART_write() and UART_read() to send and receive the data to and from other chip.
Does it have any solution to open UART2 successfully? Then send and receive data throught this UART2.
void UART2_Init(uint32_t baud, uint32_t timeout)
{
UART_HwAttrs uart_cfg_cfgtool;
UART_Params params;
UART_socGetInitCfg(UART_FOR_FSOE, &uart_cfg_cfgtool);
UART_socSetInitCfg(UART_FOR_FSOE, &uart_cfg_cfgtool);
UART_Params_init(¶ms);
params.baudRate = baud;
params.stopBits = UART_STOP_ONE;
params.readDataMode = UART_DATA_BINARY;
params.writeDataMode = UART_DATA_BINARY;
params.readReturnMode = UART_RETURN_FULL;
params.readEcho = UART_ECHO_OFF;
params.readTimeout = timeout;
uart_handler = UART_open(2, ¶ms);
if(uart_handler == NULL)
{
printf("uart2 open fail");
}
}
These are the library version I use.

Look forward to hearing your advice. Thanks a lot.
Kind regards,
Sandro