This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM355SDK783911 build

Dear all,

I have build successfully the DM355SDK783911.Below are the contents of DM355SDK783911/image directory
Please verify if i have build successfully.For fsimage and fsimage.uImage(in bold below) the size showing is 0 kb.
Is it because that i haven't build successfully or is it alright.


-rwxr-xr-x 1 root root  180052 2011-06-21 10:58 bootloader
-rw-r--r-- 1 root root  182272 2011-06-21 10:58 bootloader.nandbin
-rw-r--r-- 1 root root   58781 2011-06-21 10:04 bspconfig
-rw-r--r-- 1 root root     170 2011-06-21 10:57 cmdline
-rw-r--r-- 1 root root       0 2011-06-21 10:57 fsimage
-rw-r--r-- 1 root root       0 2011-06-21 10:58 fsimage.uImage

lrwxrwxrwx 1 root root       7 2011-06-21 10:11 kernel -> vmlinux
-rw-r--r-- 1 root root 3250608 2011-06-21 10:58 kernel.uImage
-rwxr-xr-x 1 root root   13188 2011-06-21 10:57 ubl
-rw-r--r-- 1 root root   16384 2011-06-21 10:58 ubl.nandbin
-rwxr-xr-x 1 root root  180064 2011-06-21 10:57 upgrade_bootloader.bin
-rwxr-xr-x 1 root root 3250544 2011-06-21 10:11 vmlinux


Also please find the size of /srv/tftp dir
-rw-r--r-- 1 root root  182272 2011-06-21 10:58 bootloader.nandbin.root.

leopard
-rw-r--r-- 1 root root       0 2011-06-21 10:58 fsimage.uImage.root.leopard
-rw-r--r-- 1 root root 3250608 2011-06-21 10:58 kernel.uImage.root.leopard
-rw-r--r-- 1 root root   16384 2011-06-21 10:58 ubl.nandbin.root.leopard
-rwxr-xr-x 1 root root  180064 2011-06-21 10:58 upgrade_bootloader.bin.root.leopard

In this also the same problem fsimage.uImage is 0 kb.

If the build i got is right i want to install the images on the board(LeopardBoard DM355).Please tell
me the procedure for doing the same.

Thanking all of you for your help.


Thanks and Regards,
Mayank Agarwal

  •  

     

    Hi,

    I have built the DM355SDK789311 and the contents of images folder is below:

    -rwxr-xr-x 1 root root  180052 2011-06-21 10:58 bootloader
    -rw-r--r-- 1 root root  182272 2011-06-21 10:58 bootloader.nandbin
    -rw-r--r-- 1 root root   58781 2011-06-21 10:04 bspconfig
    -rw-r--r-- 1 root root     170 2011-06-21 10:57 cmdline
    -rw-r--r-- 1 root root       0 2011-06-21 10:57 fsimage
    -rw-r--r-- 1 root root       0 2011-06-21 10:58 fsimage.uImage
    lrwxrwxrwx 1 root root       7 2011-06-21 10:11 kernel -> vmlinux
    -rw-r--r-- 1 root root 3250608 2011-06-21 10:58 kernel.uImage
    -rwxr-xr-x 1 root root   13188 2011-06-21 10:57 ubl
    -rw-r--r-- 1 root root   16384 2011-06-21 10:58 ubl.nandbin
    -rwxr-xr-x 1 root root  180064 2011-06-21 10:57 upgrade_bootloader.bin
    -rwxr-xr-x 1 root root 3250544 2011-06-21 10:11 vmlinux

     

    Does anyone know how can i install the images on Leopardboard DM355.

    Please point me to any urls or the complete procedure for doing the same.

    Thanks and Regards,

    Mayank