Part Number: AM4376
Hi Support Team,
GPMC Pin Multiplexing Options: MultiplexedAddress Data 16-Bit Device, when selecting
Note (1) in Table 9-5. GPMC Pin Multiplexing Options in the TRM states the following
(1) The values in this column represent the signals on the memory.
Be aware that some 16-bit memories may label the addresslines differently.
Some label the LSB as A0, while others use A1 for the LSB. These columns assume the LSB is A0.
Am I correct in assuming that the notes here are as follows?
Best Regards,
Kanae