This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: DSS M2M writeback mode (M2M) in linux SDK

Part Number: TDA4VM
Other Parts Discussed in Thread: AM5718,

Hello,

I see from the SDK documentation that writeback (M2M) mode on the DSS is available for the processor SDK RTOS, but it isn't enabled for the Linux SDK. Is there a way to enable this functionality within Linux? I have a customer using AM5718 today using the VPE to process one video stream and scale it and colorspace correct the video data before sending it out across either Ethernet or USB interfaces. It seems like the only way to do this on TDA4VM would be if there was a way to leverage the writeback mode to send the converted frame back to memory so that it could be accessed by different interfaces other than the display output.s 

Would there be another way to accomplish this functionality?

Munan