Hi.
When assigning the "Q"SPI for TDA4, which syscofig item I can choose from the attached pic?
SPI? I think this is not correct.
But which one?
BR Rio
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi BC.
In the TDA4 DS, it told us this:
– One OSPI and one QSPI flash interfaces
– One HyperBus and one QSPI flash interface
So, we need to use the MCI_FSS0_OSPI for QSPI and OSPI?
May you point out which pin used for the OSPI as well?
BR Rio