Other Parts Discussed in Thread: AM3517
Hello:
I am new to TI development of the Logic PD - Zoom AM3517 eXperimenter Kit. I would to flash the WinCE 6.0 BSP into NAND flash. I want to have the entire CPU board boot up and run out of the NAND flash. In WinCE 6.0, the first step is to flash XLDR and Eboot into NAND flash. I try to switch the AM3517 boot loader into internal ROM to program the XLDR and EBOOT, but fail to get the AM3517 into internal boot. I had tried the switch S2 (boot) configuration, but fail internal boot.
What jumper/S2 switch to get the ZOOM AM3517 eXperimenter Kit inorder to use PSERIAL to flash the XDLR and EBOOT (RAW) into NAND flash?
Development board specification:
* Zoom™ AM3517 eXperimenter Kit
* The AM3517 SOM-M2 supports the Texas Instruments Sitara AM3517 microprocessor with ARM Cortex-A8 RISC core running at 600 MHz
- 256 MB DDR2 SDRAM
- 512 MB NAND flash
- Wired Ethernet
- http://www.logicpd.com/products/development-kits/zoom-am3517-experimenter-kit#tabs-som-2
Mike