Other Parts Discussed in Thread: UNIFLASH, SYSCONFIG
Hi,
I'm trying to build and flash the R5F Hello world application on that EVM.
I'm following that guide:
https://software-dl.ti.com/mcu-plus-sdk/esd/AM64X/latest/exports/docs/api_guide_am64x/EVM_SETUP_PAGE.html
I encounter the following error:
C:\ti\mcu_plus_sdk_am64x_08_03_00_18\tools\boot> python uart_uniflash.py -p COM4 --cfg=sbl_prebuilt/am64x-evm/default_sbl_null.cfg Parsing config file ... Parsing config file ... SUCCESS. Found 2 command(s) !!! Executing command 1 of 2 ... Found flash writer ... sending sbl_prebuilt/am64x-evm/sbl_uart_uniflash.release.tiimage Sent flashwriter sbl_prebuilt/am64x-evm/sbl_uart_uniflash.release.tiimage of size 286189 bytes in 28.62s. Executing command 2 of 2 ... Command arguments : --file=sbl_prebuilt/am64x-evm/sbl_null.release.tiimage --operation=flash --flash-offset=0x0 Sending sbl_prebuilt/am64x-evm/sbl_null.release.tiimage: 1%|▌ | 2058/264685 [00:02<12:05, 361.80bytes/s]send error: expected ACK; got b'\x18' for block 2 Sending sbl_prebuilt/am64x-evm/sbl_null.release.tiimage: 1%|▊ | 3087/264685 [00:03<03:25, 1272.86bytes/s]send error: expected ACK; got b'\x18' for block 2 Sending sbl_prebuilt/am64x-evm/sbl_null.release.tiimage: 2%|█ | 4116/264685 [00:03<03:24, 1272.86bytes/s]send error: expected ACK; got b'0' for block 2 Sending sbl_prebuilt/am64x-evm/sbl_null.release.tiimage: 2%|█▍ | 5145/264685 [00:03<03:23, 1272.86bytes/s]send error: expected ACK; got b'2' for block 2 Sending sbl_prebuilt/am64x-evm/sbl_null.release.tiimage: 2%|█▋ | 6174/264685 [00:03<01:25, 3021.16bytes/s]send error: expected ACK; got b'0' for block 2 Sending sbl_prebuilt/am64x-evm/sbl_null.release.tiimage: 3%|█▉ | 7203/264685 [00:03<01:25, 3021.16bytes/s]send error: expected ACK; got b'0' for block 2 Sending sbl_prebuilt/am64x-evm/sbl_null.release.tiimage: 3%|██▏ | 8232/264685 [00:03<01:01, 4150.79bytes/s]send error: expected ACK; got b'0' for block 2 Sending sbl_prebuilt/am64x-evm/sbl_null.release.tiimage: 3%|██▌ | 9261/264685 [00:03<01:01, 4150.79bytes/s]send error: expected ACK; got b'0' for block 2 Sending sbl_prebuilt/am64x-evm/sbl_null.release.tiimage: 4%|██▊ | 10290/264685 [00:03<00:47, 5327.56bytes/s]send error: expected ACK; got b'0' for block 2 Sending sbl_prebuilt/am64x-evm/sbl_null.release.tiimage: 4%|███ | 11319/264685 [00:03<00:47, 5327.56bytes/s]send error: expected ACK; got b'0' for block 2 Sending sbl_prebuilt/am64x-evm/sbl_null.release.tiimage: 5%|███▎ | 12348/264685 [00:03<00:38, 6484.41bytes/s]send error: expected ACK; got b'0' for block 2 send error: NAK received 11 times, aborting. Sending sbl_prebuilt/am64x-evm/sbl_null.release.tiimage: 5%|███▎ | 12350/264685 [00:03<00:38, 6484.41bytes/s] [ERROR] XMODEM send failed, no response OR incorrect response from EVM OR cancelled by user, Power cycle EVM and run this script again !!!
I try to power cycle the board and restart the serial connection but the problem remains.
Setup Details:
- OS: win 10
- CCS 12.1.0.00007
- Python 3.11.0
- MCU+ SDK: 8.3.0.18
- SysConfig 1.14.0
- XDCtools 3.62.1.16_core
- TI Clang v2.1.2.LTS
- GNU v7.2.1
- PRU TI v2.3.3
Thanks