Part Number: OMAP-L138
Other Parts Discussed in Thread: OMAPL138
The dependency of out2rprc.exe on .NET 3.5 creates issues.
We have incorporated out2rprc.exe in post-build steps in projects for the C674x core of the OMAP-L138.
We use out2rprc.exe to take the .out file and create a .bin file.
We append a CRC32 checkvalue to the file and load it into NAND Flash.
We based our OMAP-L138 ARM core userbootloader on the LCDK bootloader project in OMAPL138_StarterWare_1_10_04_01
Our userbootloader loads the memory sections stored in the *.bin file in NAND Flash.
That all has been working fine for years.
Lately, if we set up Code Composer Studio on a new workstation, out2rprc.exe will fail to run until we install .NET 3.5
I have learned recently that folks are having trouble using out2rprc.exe on a Windows build server because they cannot install .NET 3.5.
Are there options to move forward?
Alternative to out2rprc.exe for the C674x core of the OMAP-L138?
A way to rebuild out2rprc.exe so it can run on a Windows build server?