This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Drivers for TNET1130 WLAN Adapter

I lost the driver cd for this adapter and really badly need the drivers, can someone point out where to get them?

I have tried everywhere, hope someone can help.

  • Thomas, I am going to move this post to the High Performance C6000 DSPs forums where someone will likely be able to help.

  • The unfortunate situation is that the TNETW1130 product line was sold to Infineon in August 2007.

  • Normal 0 false false false MicrosoftInternetExplorer4

    Hi All,

    I have had success loading drivers with my TNET1130 PCI wireless card. The back ground of this hardware is:- I bought it off ebay in the UK possible in 2008. It has a label with the words 'Long Range Wireless PCI Network Card TNET1130' stuck over the screen which covers the miniPCI card. The minPCI card is type XG-650.

     The driver installed is called 'NB 802.11g Wireless Network PCI Adaptor (1130) issued 10-Dec-2004 version 7.0.1.33 . I down loaded it from http://www.billion.uk.com/esupport/index.php?_m=downloads&_a=viewdownload&downloaditemid=10&nav=0,47,6 . If this link goes old I suggest you search 'XG_950WPA2_U2.0.0.2F2.0.0.2O2.0.0.2D7.0.1.33.zip www.billion.uk.com'. The diver is listed to work with W98, W2K and XP. It comes with utilities and an installation guide. I didn't install the utilities, I am using windows resident 'wireless networks' to manage the card. It is working reliably with WPA-PSK TKIP data encryption.

     From the name of the download file I would like to suggest that the older drivers for XG-950 wireless PCI cards are suitable for use with the XG-650 wireless PCI card. The XG-950 was designed for a 108M bps. The XP-650 was designed for 54M bps. But test them at YOUR OWN RISK. I didn’t get it right first time. You should make ‘systems restore points’ before attempting to load any software if you are nervous.

     The XG-950 driver Version 7.0.1.33 10-December-2004 works well on my 32bit XP machine with the XG-650 TNET1130 wireless PCI card.