This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Enable the TI4818 EDMA clocks



I am using the EDMA3 for data transfer with McASP port. But i am not able to access the EDMA configurations ( content of CC and TC memory are 0xBAD0BAD0, from 0x49000000 from A8). I believe the clock for EDMA CC and TC are not enabled.

How do i enable the TI4818 EDMA clocks?  The code below does not seem to be enough:

#define CM_DEFAULT_L3_FAST+CLKSTCTRL 0x48180508

#define CM_DEFAULT_DMM_CLKCTRL  0x48180528

 WR_MEM_32(CM_DEFAULT_L3_FAST_CLKSTCTRL, 0x2); /*Enable the Power Domain Transition of L3 Fast Domain Peripheral*/
 WR_MEM_32(CM_DEFAULT_DMM_CLKCTRL,       0x2); /*Enable EMIF1 Clock*/

Thanks in advance,

Philip