This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM648 and NDK version 2



hola ;

The board which i am currently working on is DM648 . A little introduction on the board , it consist of two ethernet physicals on board and both can be used simltaneously due to CPSW module . The Gigabit switch , performs switching betwwen the two ethernet physicals .

Now the are two modes of etherent transfer , one is normal mode or by pass mode.

Can anyone xplain th normal mode ? because the document doesnt describes it and only the name is mentioned.

The ndk version 2 provides different ethernet xamples . One of which is Hello world , i wanted to ask in this xample project how is the switch configured in the normal or bypass mode?

Now the ndk project can be modified according to user needs. But i am not sure how to do that because the helloworld project import a lot of libraies in the workspace. Now the function i want to change  are also present in libraries . Can anyone tell me how to resolve this problem of libraries and change code according to my need ?

If someone has worked on DM648 ethernet physical , please share what you have achieved and how did you accomplished it for it will be great help to me and my project.

Thank you

Amna