Other Parts Discussed in Thread: TMS320DM642, TMS320DM648
hello
I am working on DM648 , and read the article Software Migration From TMS320DM642 to
TMS320DM648/DM6437 (SPRAAX5). What am I interested is to configure the Ethernet module of DM648 , I have no example in pspdrivers – driver folder and there is no mention of configuration of emac module in the pspdrivers – soc Folder.
So I my project is in standstill position, I have to configure the emac module and establish full duplex communication via DM648. Kindly tell me where to begin…..
The ndk example , HELLOWORL.prj establish the full duplex communication but I cannot see in which part of memory is storing the received packets where does is it transmitting packet is being stored.
I would like to see each packet being received Ethernet jack, please help me in completing this task.
Regards
Amna