This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EDMA 1-D data transfer issue in C6713

Hi,

In my design, the McASP is connected to a 6-channel ADC through a McASP.

I have configured the McASP in synchronous TDM mode and wanted to configure

EDMA to transfer the data received from the McASP port to a variable in CE0 space.

The CE0 space is connected to a FPGA. And there is code in FPGA which takes the EMIF signals

and acts as a asynchronous SRAM.

 

This is how I have configured my EDMA port.

    /* Configure EDMA parameters */
    
      EDMA_configArgs(
          hEdmaAREVT,    
          EDMA_OPT_RMK(
               EDMA_OPT_PRI_HIGH,
               EDMA_OPT_ESIZE_16BIT,    /* Element size 16 bits */
               EDMA_OPT_2DS_NO,
               EDMA_OPT_SUM_NONE,
               EDMA_OPT_2DD_NO,
               EDMA_OPT_DUM_INC,
               EDMA_OPT_TCINT_YES,      /* Enable Transfer Complete Interrupt    */
               EDMA_OPT_TCC_OF(edmaChaAREVT),
               EDMA_OPT_LINK_NO,       /* Enable linking to NULL table          */
               EDMA_OPT_FS_YES
               ),
           EDMA_SRC_RMK(MCASP_getRbufAddr(hMcasp)),      
           EDMA_CNT_OF(0x00000006),/* no. of elements   */
           EDMA_DST_RMK((int32_t)RxData),
           EDMA_IDX_OF(0x00000000),
           EDMA_RLD_OF(0x00060000)
     );     
                        
     /* Enable EDMA interrupts */
     EDMA_intDisable(edmaChaAREVT);
     EDMA_intClear(edmaChaAREVT);
     EDMA_intEnable(edmaChaAREVT);   

     /* enable EDMA channels */ 
     EDMA_enableChannel(hEdmaAREVT);

The main aim is to transfer the 6 TDM data words from the McASP to the CE0 locations continuously.

But in the CE0 space, I am able to receive only one word. while I want to receive all the 6 data words

in contiguous address locations (see parameter INC in OPT register, DUM bit).

Could somebody please suggest if there is something I am missing in the EDMA configuration. Please guide.

 

Thanks,

Aditi.