Part Number: AM625
Hi Ti,
Iam getting below issue , could you please help me on this.
root@am62xx-evm:~# weston
Date: 2022-12-07 UTC
[08:42:30.822] weston 8.0.0
wayland.freedesktop.org
Bug reports to: gitlab.freedesktop.org/.../
Build: 8.0.0
[08:42:30.822] Command line: weston
[08:42:30.822] OS: Linux, 5.10.109-g9e58028f94, #28 SMP PREEMPT Fri Sep 30 14:34:37 IST 2022, aarch64
[08:42:30.823] Using config file '/etc//weston.ini'
[08:42:30.823] Output repaint window is 7 ms maximum.
[08:42:30.823] Loading module '/usr/lib/libweston-8/drm-backend.so'
[08:42:30.829] initializing drm backend
[08:42:30.830] logind: failed to get session seat
[08:42:30.830] logind: cannot setup systemd-logind helper (-61), using legacy fallback
[08:42:30.830] failed to get VT mode: Inappropriate ioctl for device
[08:42:30.830] fatal: drm backend should be run using weston-launch binary, or your system should provide the logind D-Bus API.
[08:42:30.830] fatal: failed to create compositor backend
Internal warning: debug scope 'drm-backend' has not been destroyed.
Thanks,
Naresh