Hi,
Ocasionally, when running the Hello World NDK example from the MCSDK Beta-2 on the C6670 EVM lite, I get the following some unexpected output relating to the queues (see in bold).
The example seems to still work afterwards. Btw, this doesn't always happen.
[C66xx_0] TCP/IP Stack 'Hello World!' Application
[C66xx_0] QMSS successfully initialized
[C66xx_0] CPPI successfully initialized
[C66xx_0] PASS successfully initialized
[C66xx_0] Ethernet subsystem successfully initialized
[C66xx_0] eventId : 48 and vectId : 7
[C66xx_0] Verify_Init: Expected 0 entry count for Queue number = 912, found 1 entries
[C66xx_0] Verify_Init: Expected 0 entry count for Queue number = 913, found 1 entries
[C66xx_0] Registration of the EMAC Successful, waiting for link up ..
[C66xx_0] Network Added: If-1:192.168.2.100