What error tolerance, error concealment, and/or error resilience do the TI provided codecs for the DM648 have?
The application is streaming where bits/packets may be lost in transit. The decoder should recover from errors.
Is it better to go with the 6437 and use the TMDH264D H264 MP? http://focus.ti.com/docs/toolsw/folders/print/tmdh264d.html.
Does TI have any plans to make the above codec available for the DM648? If not, is the h264 BP codec a better choice, with respect to error resilience, than the MPEG4 codec (mpeg4dec)?