Other Parts Discussed in Thread: TVP5158
Hello,
I'm using TVP5158 for capturing 4 channel (all NTSC or all PAL) on DM6467 in 4-ch interleaved mode. In some cases it happens that a horizontal line appears on the acquired video and shifts upwards in the following frames and then starts back from the bottom. This effects happens on all the four channels. Analysing the frames I noticed that the horizontal line is taken from a channel different from the correct channel. The lines are swapped in the frames. The problem seems to be in the de-interleaving procedure from the superframe to the four frame buffers. It seems that a wrong channel number is associated to some lines in the metadata of the superframe, so the lines are swapped from a frame to another one and viceversa in de-interleaving process. Resetting the TVP5158 the problem disappears.
Am I missing any configuration?
Thanks,
Luca