This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCI6484 Configuration file and NDK version?

Hi,

has someone already have experience with the tci6484 board?

I want to create a project with a configuration file, but I don't know which platform I should select to create the file.

Is it based on c6455, so that I can use the "ti.platforms.dsk6455.sch" file?

Which NDK version should I use? I have installed the 2.0.0.0 version, but it has no example application for tci6484.

There is only a tci6488 folder.

I am happy about any help!

 

Regards,

Ruba