This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8168 recommended RAM volume

Other Parts Discussed in Thread: TVP5158

I'm working on a design with the DM8168 and am unsure about the amount of RAM we should use. 

We need to do at least the following:

* Take 720p in one of the "video in" ports, encode it to H.264, put it in a transport stream and send it out the network via RTP.

* Take 3 channels of standard definition video in via the TVP5158, convert it from PAL to NTSC, scale it to 720p, encode it to H.264, put it in a transport stream and send each of the 3 out the network via RTP with accompanying audio.

* Take one 720p H.264 file with audio, decode it and display it out a standard definition output and analog audio output.

* NFS mount remote filesystems for file access.

I noticed that the EVM has 1GB of RAM.  Also, Z3 makes a module with 512MB or 1GB of RAM.  Is there a reason that these devices have so much?

If I look at some of the documents included with the EVM, I see numbers describing the RAM required to do an encode or decode, but this is only a small piece of the full equation, right?  Is there any good rule of thumb for determining how much RAM should be used?