Other Parts Discussed in Thread: AM1808
Hello, I didn't think it was possible for things to get any worse from yesterday, but they have...
I have a TI816x/389x EVM rev D (with DIMM) board. It came with a XDS100v2.
1) In the process of trying to build and program a u-boot (nand) for DDR2 the board will not do anything now. Won't even boot the original CF card supplied. Nothing prints to the console at all. Jumpers look correct. What could have happened where nothing will boot/print. Can it be recovered?
2) Can't connect to target with the emulator anymore (could yesterday) IcePick_D_0: Error connecting to the target: (Error -180) @ 0 (0x0) What does this error mean?
3) The CF card has a CCS5 version on it that does not seem to have support for the TI816x (board that it was shipped with). What CCS version should I use? The only version that seems to have support for the Ti816x/xds100v2 is 5.0.1.201105110900. All doc show the use of the xds560 emulator with this board. Is what we were sent even a valid configuration? Been tested?
4) I have 2 different ezsdk versions. ezsdk_c6a816x and ezsdk_dm816x. Which one should I be using? The C6a816x seems to not have the DDR3/2 issues, but does not include the host_tools dir.
5) When I could connect to the board, i could not read the the device ID of the Nand chip correctly.
Any help would be greatly appreciated.
Thanks, Michael