Other Parts Discussed in Thread: CCSTUDIO
I'm having problems with the loading for an out file generated by Code composer 3.3.
When I load an out file generated by Code Composer 2.2 VIA my own application (platform: Window XP sp3, Visual studio 2005), I see that it works ok.
However, when I try to load and out file which was build with Code Composer 3.3 i see that it is not doing what it should do (turn leds on).
I heard that there was some change in the out file form between CC.2.x and CC.3.x.
Is anyone here familier with this problem? How can I solve is (or bypass it