Part Number: AM3356
Hi Champs,
Is it safe to power up/down 1.35V DDR3L rail at the same time as the 3.3V, 1.8V rails?
From this figure, it seems it would be possible, but want to confirm:

BR,
-RT
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Additionally, is there additional powerup/powerdown recommendations on max voltage difference between the following?
Thank you!
-RT
Hello Ryan T,
Thank you for the query.
Since i am not aware of the power solution you are using, i would say if you are following the sequence recommended in the datasheet that should be fine.
There are different power sequences available and alternate power-supply sequence is one of them.
Regarding the time duration between supply rails, we do not have a time number. It is important to follow the sequencing and ensure that the device is held in reset until all the supply rails and the oscillator are stable. This is shown in the power sequence diagrams.
Regards,
Sreenivasa