This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6474 SRIO boot mode

To whom it may concern:

                 I encounter a problem when booting the c6474 with srio boot mode,As the C6474`s PDF information has said, when booting the c6474, the device ID of the C6474 is determined by the bootmode[2] and CFGGP[2:0], device ID =2+bootmode[2] :CFGGP[2:0], bootmode[3:0] =0b1011,and the CFGGP[3:0]=0b0001,so the device ID of the C6474 is 3,but after the c6474 is configured with SRIO boot mode, the BASE_ID=0xFFFFFF when I read from its address 0x02d01060,and if I send a maintenance packet to read its BASE_ID(offset is 0x60),an error occurs,I do not known why it is?

                 Thank you for attention! I am very anxious to get answered.

xiaoyan