This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-AM437X: Flash Erase Inconsistency

Part Number: PROCESSOR-SDK-AM437X
Other Parts Discussed in Thread: UNIFLASH

When attempting to flash erase QSPI on our board, sometimes the erase is successful but other times it fails. The observation is that when it erases successfully, the command will remain in "Header Transfer Complete!!" as seen in the following image. Which would then eventually report a "Flash Erase Success!"

We observe that when the erase is not good, the status appears very fast as seen in the following image:

We can confirm the success of the flash erase when loading the app image since it will load up to 100% when flash erases was truly successful. On the other hand, when the flash erases was not good then when loading the app image, it will only reach 1% and fail.

The question is: Why is it that once seeing "header Transfer Complete!", then "Flash Erase Success!" appears right after without delay?