This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM355SDK783911 handshaking error



 

Hello all,

 

i am trying to build DM355SDK789311 using sudo make installbootloader VERBOSE=1 but i am getting handshaking error as given below.In minicom on the board when i am giving the command printenv i am getting the following output:

DM355 LEOPARD# printenv                      

                                  
bootdelay=3                                                                    
baudrate=115200                                                                
bootfile="uImage"                                                              
addip=setenv bootargs ip=dhcp mem=80M console=ttyS0,115200n8 root=/dev/ram0 rw =
bootargs=console=ttyS0,115200n8 root=/dev/ram0 rw initrd=0x82000000,11M mem=60Mn
filesize=2bf60                                                                 
fileaddr=82000000                                                              
ipaddr=10.17.8.131                                                             
serverip=10.17.8.125        
                                                   
autostart=no                                                                   
stdin=serial                                                                   
stdout=serial                                                                  
stderr=serial                                                                  
ver=U-Boot 1.2.0 (Mar  9 2009 - 22:21:30)LEOPARD-1.0.0                         
                                                                               
Environment size: 496/16380 bytes

Please not that in above in bold the ipaddr and server ip both start with 10.

Now when i give the command sudo make installbootloader VERBOSE=1 on DM355SDK789311 i am getting the following output:
- Hide quoted text -



mayank@mayank-laptop:~/DM355SDK789311$ sudo make installbootloader VERBOSE=1
  Ridgerun Linux SDK
  Board configuration: Leopard Board
 
echo -e "\040" Installation system of uboot images over TFTP for host 10.17.8.125
  Installation system of uboot images over TFTP for host 10.17.8.125
echo -e "\040" Please be sure u-boot is running on port "/dev/ttyUSB0" and none process \(like minicom\) is using it
  Please be sure u-boot is running on port /dev/ttyUSB0 and none process (like minicom) is using it
if [ -n "`lsof -t "/dev/ttyUSB0"`" ] ; then \
        echo -e "\040" "\033[31mError: u-boot "/dev/ttyUSB0" port in use\033[0m\n"; \
        lsof "/dev/ttyUSB0"; \
        exit -1; \
    else \
        echo -e "\040" "u-boot port "/dev/ttyUSB0"\n"; \
    fi
  u-boot port /dev/ttyUSB0

cd /home/mayank/DM355SDK789311/installer/u-boot-installer/ ; perl installer bootloader
  Performing handshake with u-boot...done.

Uboot prompt: [DM355 LEOPARD# ]
  Trying to identify NAND block size... Sending [nand info]
nand size before regular expression: [NAND 256MiB 3,3V 8-bit, sector size 128 KiB
DM355 LEOPARD# ]nand size after match for old uboot nand info: [NAND 256MiB 3,3V 8-bit, sector size 128 KiB
DM355 LEOPARD# ]no match, trying new output formatnand size after match for new uboot nand info: [128]detected 0x20000

  Loading upgrade bootloader version...
  Disabling boot command...
    Uboot <= setenv bootcmd
Sending [setenv bootcmd]
  Disabling autostart option...
    Uboot <= setenv autostart no
Sending [setenv autostart no]
    Uboot <= saveenv
Sending [saveenv]
  Loading bootloader...
  Configuring the network...
    Uboot <= setenv ipaddr 192.168.1.50
Sending [setenv ipaddr 192.168.1.50]
    Uboot <= setenv serverip 10.17.8.125
Sending [setenv serverip 10.17.8.125]

    Uboot <= mw.l 0x82000000 0xff 0x100000
Sending [mw.l 0x82000000 0xff 0x100000]
    Uboot <= tftp 0x82000000 upgrade_bootloader.bin.root.leopard
Sending [tftp 0x82000000 upgrade_bootloader.bin.root.leopard]
-------------> Error: didn't match [DM355 LEOPARD# ]  Running upgrade bootloader...
Sending [go 0x82000000]
    Uboot => go 0x82000000

  Performing handshake with u-boot...
  ERROR: failed to perform handshake with u-boot.
  Be sure u-boot is active on port /dev/ttyUSB0 and you have terminal programs like minicom closed.

Exit: -1
make: *** [installbootloader] Error 255
mayank@mayank-laptop:~/DM355SDK789311$


As displayed in bold above the ipaddr is 192.168.1.50 which is different from the ipaddr in DM355SDK783911.Could this be the issue why the handshaking error is coming.

If anyone could help me  on this.

Thanking all of you for help.



Thanks and Regards,
Mayank