Hello,
I am using a simulator with CCS 3.3. The code that I am using is follow:
#include <std.h>
#include <log.h>
#include "Configuration1cfg.h"
void main()
{
}
void Task1(Arg arg1)
{
int i;
for(i=0;i<100;i++)
{
TSK_sleep(100);
LOG_printf(&trace,"In task %d\n",i);
}
}
The problem that I have is as follow:
I cannot see the output of LOG_printf in trace window until I stop the running program. I want to see the output as it is generated by program. Is there any way that I can see the trace output without stopping the program?
I tried the following code without any success:
TSK_disable();
IDL_run();
TSK_enable();
Any suggestion?
Best regards