Hi All,
I couldn't find the fields description of the PINCNTL registers in the TMS320DM814x technical reference, where this should be?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi All,
I couldn't find the fields description of the PINCNTL registers in the TMS320DM814x technical reference, where this should be?
it contains the first 8 bits only of the PINCNTL which are the MUXMODE, where is the description of the other bits. It is 32 bits register.
Here is the description of the other bits:
31:18 Rsvd Reserved
17 PULLTYPESEL Pad Pullup / Pulldown Type Selection (0 = Pulldown selected, 1 = Pullup selected)
16 PULLUDEN Pad Pullup / Pulldown Enable (1 = Pullup / Pulldown disabled, 0 = Pullup / Pulldown enabled)
15:8 Rsvd Reserved
7:0 MUXMODE Pad Functional Signal Mux Select
Regards,
Marc