Other Parts Discussed in Thread: AM1808
Hi,
We are facing some issue with AM1808. After u-boot, it is trying to load the kernel image from TFTP. We configured all the environment variables in the target and host.
we are not able to load uImage through TFTP, even there is no LED indication between Baseboard to RJ45 connections. Till yesterday it was up, but today is not working.
while connecting to target board giving below status :-
---------------------------------------------------------------
Booting with TI UBL
Device OPP (300MHz, 1.2V)
U-Boot 2009.11 (Mar 25 2010 - 14:39:42)
I2C: ready
DRAM: 64 MB
In: serial
Out: serial
Err: serial
ARM Clock : 300000000 Hz
DDR Clock : 132000000 Hz
Net: Ethernet PHY: GENERIC @ 0x00
Hit any key to stop autoboot: 0
Unknown command 'static' - try 'help'
Using device
TFTP from server 192.168.1.200; our IP address is 192.168.1.100
Filename 'uImage'.
Load address: 0xc0700000
Loading: WARN: emac_send_packet: No link
T WARN: emac_send_packet: No link
WARN: emac_send_packet: No link
WARN: emac_send_packet: No link
T WARN: emac_send_packet: No link
T WARN: emac_send_packet: No link
---------------------------------------------------------------
Any problem with RJ45 connector or Ethernet IC. Can you give me your suggestions.
Regards,
Francis