Part Number: AM6442
Other Parts Discussed in Thread: AM6422
Hello
I have AM6422 board. I using os build with Yocto. I try to boot my board over ethernet. I setup dhcp and tftp server. When board started to download tispl.bin the error occurred:
am65_cpsw_nuss_port ethernet@8000000port@2: phy_startup failed
am65_cpsw_nuss_port ethernet@8000000port@2: am65_cpsw_start end error
I figure it out that this error message is thrown in am65-cpsw-nuss.c in
...
ret = phy_startup(priv->phydev);
if (ret) {
dev_err(dev, "phy_startup failed\n");
goto err_dis_rx;
}
...
The phy_startup() function is defined in drivers/net/phy/phy.c and it calls function pointer which points to genphy_startup which finally calls genphy_update_link(). The exact error is thrown in while loop:
int genphy_update_link(struct phy_device *phydev)
{
unsigned int mii_reg;
/*
* Wait if the link is up, and autonegotiation is in progress
* (ie - we're capable and it's not done)
*/
mii_reg = phy_read(phydev, MDIO_DEVAD_NONE, MII_BMSR);
/*
* If we already saw the link up, and it hasn't gone down, then
* we don't need to wait for autoneg again
*/
if (phydev->link && mii_reg & BMSR_LSTATUS)
return 0;
if ((phydev->autoneg == AUTONEG_ENABLE) &&
!(mii_reg & BMSR_ANEGCOMPLETE)) {
int i = 0;
printf("%s Waiting for PHY auto negotiation to complete",
phydev->dev->name);
while (!(mii_reg & BMSR_ANEGCOMPLETE)) {
/*
* Timeout reached ?
*/
if (i > (PHY_ANEG_TIMEOUT / 50)) {
printf(" TIMEOUT !\n");
phydev->link = 0;
return -ETIMEDOUT;
}
if (ctrlc()) {
puts("user interrupt!\n");
phydev->link = 0;
return -EINTR;
}
if ((i++ % 10) == 0)
printf(".");
mii_reg = phy_read(phydev, MDIO_DEVAD_NONE, MII_BMSR);
mdelay(50); /* 50 ms */
}
printf(" done\n");
phydev->link = 1;
} else {
/* Read the link a second time to clear the latched state */
mii_reg = phy_read(phydev, MDIO_DEVAD_NONE, MII_BMSR);
if (mii_reg & BMSR_LSTATUS)
phydev->link = 1;
else
phydev->link = 0;
}
return 0;
}
It seems that function phy_read return incorrect value. I also tried to patch the code and replace MDIO_DEVAD_NONE with MDIO id 0x1f for DP83867 phy device but this not resolve the issue. My questions are:
1. Why MDIO_DEVAD_NONE is used? This is not correct MDIO id for this device
2. This problem also appears on SDK image. How to solve it?
And question less related to topic:
1. What is the purpose ot tiboot3.bin firmware?
Thank you for response
BR
Jakub