Part Number: AM625
Customer have question regarding the MCU_OSC0_XI input. They plan to use and LVCMOS oscillator, but it looks like for the application were are limited by the fact the oscillator output can only run as low as 2.5V. They cannot change that due to some supply constraints at the moment. From reading the spec, it looks like this signal is internally AC-coupled. Any concern about using a resistor divider to level shift from 2.5V to 1.8V?
Also any concern to the rise/fall times the MCU_OSC0_XI input as the datasheet does not have it spec’d and when they are thinking of putting a resistor divider here.