Part Number: TMDS64GPEVM
Hi Team,
I compiled U-BOOT according to this: https://software-dl.ti.com/processor-sdk-linux/esd/AM64X/latest/exports/docs/linux/Foundational_Components/U-Boot/UG-General-Info.html#getting-the-u-boot-source-code
Question 1: There is no ti-sysfw folder in the ti-linux-firmware after git clone. I found the required files in the prebuilt-images folder. Why are they missing? Is the tutorial on this page the latest?

Question 2: An error was reported when I was compiling it. Precisely, the error was reported at the step shown in the red box in my case.

The details of the error are as follows:
make[1]: Entering directory '/opt/ti-processor-sdk-linux-am64xx-evm-08.02.00.23/board-support/u-boot-2021.01+gitAUTOINC+44a87e3ab8-g44a87e3ab8/out/a53' GEN ./Makefile scripts/kconfig/conf --syncconfig Kconfig CFG u-boot.cfg GEN include/autoconf.mk GEN include/autoconf.mk.dep CFG spl/u-boot.cfg GEN spl/include/autoconf.mk ===================== WARNING ====================== This board uses CONFIG_SPL_FIT_GENERATOR. Please migrate to binman instead, to avoid the proliferation of arch-specific scripts with no tests. ==================================================== CFGCHK u-boot.cfg Using /opt/ti-processor-sdk-linux-am64xx-evm-08.02.00.23/board-support/u-boot-2021.01+gitAUTOINC+44a87e3ab8-g44a87e3ab8 as source for U-Boot GEN ./Makefile UPD include/generated/timestamp_autogenerated.h rm -f scripts/dtc/pylibfdt/_libfdt*.so PYMOD scripts/dtc/pylibfdt/_libfdt.so /opt/ti-processor-sdk-linux-am64xx-evm-08.02.00.23/board-support/u-boot-2021.01+gitAUTOINC+44a87e3ab8-g44a87e3ab8/scripts/dtc/pylibfdt/setup.py:21: DeprecationWarning: The distutils package is deprecated and slated for removal in Python 3.12. Use setuptools or check PEP 632 for potential alternatives from distutils.core import setup, Extension HOSTCC tools/mkenvimage.o HOSTLD tools/mkenvimage HOSTCC tools/fit_image.o HOSTCC tools/image-host.o HOSTCC tools/dumpimage.o HOSTLD tools/dumpimage HOSTCC tools/mkimage.o HOSTLD tools/mkimage CC arch/arm/cpu/armv8/fwcall.o as: unrecognized option '-EL' make[2]: *** [/opt/ti-processor-sdk-linux-am64xx-evm-08.02.00.23/board-support/u-boot-2021.01+gitAUTOINC+44a87e3ab8-g44a87e3ab8/scripts/Makefile.build:266: arch/arm/cpu/armv8/fwcall.o] Error 2 make[1]: *** [/opt/ti-processor-sdk-linux-am64xx-evm-08.02.00.23/board-support/u-boot-2021.01+gitAUTOINC+44a87e3ab8-g44a87e3ab8/Makefile:1789: arch/arm/cpu/armv8] Error 2 make[1]: Leaving directory '/opt/ti-processor-sdk-linux-am64xx-evm-08.02.00.23/board-support/u-boot-2021.01+gitAUTOINC+44a87e3ab8-g44a87e3ab8/out/a53' make: *** [Makefile:167: sub-make] Error 2
Could you please tell me how to solve this error?
Kind regards,
Katherine