This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Chip selection



Hi team,

Customers need two embedded chip and the requirements are as follows:

1) digital radio application, modulation demodulation algorithm core DSP chip:

a. Single-core 32-bit fixed-point DSP;

b. Operating frequencies greater than 100m;

c. Operating temperature -40~85;

d. 256KB SRAM+64KB DRAM integrated internally, 12KB ROM or higher

e. 3 I2S, 2 SPI, 1 UART, 1 USB or more

f. Core voltage 1-1.3C

2)  master chip Arm processor:

a. 16 bit with a main frequency greater than 150 MHz (greater than or equal to 1 core)

b. Core voltage ≤ 3.3 V, IO voltage ≤ 3.3 V.

c. Instruction cache ≥ 128 KB, data cache ≥ 128 KB

d. number of IO ≥ 80

e. number of PWM outputs ≥ 32

Could you help give some recommendations? Thanks.

Best Regards,

Cherry