Part Number: TDA4VM
Hi team,
Here's an issue from the customer may need your help:
1) Does EVM577PFUSION-V1-0 + TDA4VM support QNX+RTOS?
Customers have several carmera expansion boards (EVM577PFUSION-V1-0) and development boards for TDA4VM that they want to run QNX+Rtos systems.
They are concerned if the drive of EVM577PFUSION-V1-0 Expansion Board needs to be re-bringup.
2) Which SDK package is for the corresponding QNX+Rtos?
If the drive for the EVM577PFUSION-V1-0 expansion board is done on the Rtos side, what is the SDK download path for QNX+Rtos? They want to run the demo of vision_apps directly. The current download location for qnx+Rtos SDK is as follows:
https://www.ti.com/tool/PROCESSOR-SDK-J721E
The deployment follows the following URL:
Are there any issues with the download path above?
Could you help check this case? Thanks.
Best Regards,
Cherry