Other Parts Discussed in Thread: CCSTUDIO
When I try to run the LED example project that came with the 642 EVM I get the follwing error.
[ledprd.c] "C:\CCStudio_v3.3\C6000\cgtools\bin\cl6x" -g -q -fr"C:/CCStudio_v3.3/boards/evmdm642/examples/bsl/ledprd/Debug" -i"." -i"C:/CCStudio_v3.3/boards/evmdm642/include" -i"C:/CCStudio_v3.3/boards/evmdm642/csl/include" -d"_DEBUG" -ml3 -mv6400 -@"Debug.lkf" "ledprd.c"
"C:/CCStudio_v3.3/boards/evmdm642/csl/include/csl_chiphal.h", line 262: fatal error: #error NO CHIP DEFINED (use -dCHIP_XXXX where XXXX is chip number, i.e. 6201)
I added a #define CHIP_DM642
but then I get
<Linking>
undefined first referenced
symbol in file
--------- ----------------
_I2C_outOfReset C:/CCStudio_v3.3/boards/evmdm642/lib/evmdm642bsl.lib
_I2C_getConfig C:/CCStudio_v3.3/boards/evmdm642/lib/evmdm642bsl.lib
_I2C_start C:/CCStudio_v3.3/boards/evmdm642/lib/evmdm642bsl.lib
_GPIO_open C:/CCStudio_v3.3/boards/evmdm642/lib/evmdm642bsl.lib
_I2C_open C:/CCStudio_v3.3/boards/evmdm642/lib/evmdm642bsl.lib
_CSLDM642_LIB_ C:/CCStudio_v3.3/boards/evmdm642/lib/evmdm642bsl.lib
_CACHE_enableCaching C:/CCStudio_v3.3/boards/evmdm642/lib/evmdm642bsl.lib
_I2C_xrdy C:/CCStudio_v3.3/boards/evmdm642/lib/evmdm642bsl.lib
_I2C_bb C:/CCStudio_v3.3/boards/evmdm642/lib/evmdm642bsl.lib
_I2C_sendStop C:/CCStudio_v3.3/boards/evmdm642/lib/evmdm642bsl.lib
_EMIFA_config C:/CCStudio_v3.3/boards/evmdm642/lib/evmdm642bsl.lib
__CSL_init C:/CCStudio_v3.3/boards/evmdm642/lib/evmdm642bsl.lib
_I2C_writeByte C:/CCStudio_v3.3/boards/evmdm642/lib/evmdm642bsl.lib
_I2C_config C:/CCStudio_v3.3/boards/evmdm642/lib/evmdm642bsl.lib
_GPIO_pinRead C:/CCStudio_v3.3/boards/evmdm642/lib/evmdm642bsl.lib
_GPIO_pinEnable C:/CCStudio_v3.3/boards/evmdm642/lib/evmdm642bsl.lib
_GPIO_pinDirection C:/CCStudio_v3.3/boards/evmdm642/lib/evmdm642bsl.lib
_GPIO_pinWrite C:/CCStudio_v3.3/boards/evmdm642/lib/evmdm642bsl.lib
>> error: symbol referencing errors -
'C:/CCStudio_v3.3/boards/evmdm642/examples/bsl/ledprd/Debug/ledprd.out' not built
>> Compilation failure
I checked and C:\CCStudio_v3.3\boards\evmdm642\lib\evmdm642bsl.lib exists, so what next?