This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Raw ethernet example required on C6452???



hello;
i have DM648 board from lyrtech. but i don't need any NDK example.
i have the task to complete full duplex communication on the board. but i have no such basic example from where i can start my task.
simply i need a project that receives raw ethernet packets from one RJ45 and transmits through other RJ45 and vice versa. i have no such example provided with my board. if you have any such example either of DM648 or C6452 board, send me that.
thanks in advance.
regards
akqureshi