Hi,
I need verified TDA4VM worked as a slave device which connected to host PC (worked as master device),I know the EVM should work as PCIe End Point, From links :https://software-dl.ti.com/jacinto7/esd/processor-sdk-linux-jacinto7/08_00_00_08/exports/docs/linux/Foundational_Components/Kernel/Kernel_Drivers/PCIe/PCIe_End_Point.html I know I need to edit dts and run some command and switch the dip 3.5,3.6 to "on" which I have run ok on j721EVM. But now I need to verified the function on TDA4VM Edge AI Starter Kit platform, but i didn't find any instructions on this platform about pcie endpoint ,
Can anyone give me some helps about it? thanks!