Part Number: AM3357
Hi,
I had connected the blackhawk 560v2 usb emulator to the board. Then i am getting the following error.
[Start: Blackhawk XDS560v2-USB System Trace Emulator_0]
Execute the command:
%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
/home/atl/.ti/ccs1120/0/0/BrdDat/testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 560/2xx-class product.
This utility will load the program 'libbh560v2u.out'.
Loaded FPGA Image: /home/atl/ti/ccs1120/ccs/ccs_base/common/uscif/./dtc_top.jbc
The library build date was 'Mar 17 2022'.
The library build time was '19:00:32'.
The library package version is '9.7.0.00213'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.
An error occurred while hard opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-180' (0xffffff4c).
The title is 'SC_ERR_CTL_NO_TRG_POWER'.
The explanation is:
The controller has detected a target power loss.
The user must turn-on or connect the power supply for the target.
[End: Blackhawk XDS560v2-USB System Trace Emulator_0]
I had done this in MMC0 boot mode.
whether we have to use any other boot mode.